LS1043 platform "reset" can not work

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1043 platform "reset" can not work

Jump to solution
1,310 Views
allan_yi
Contributor I

we use LS1043,it is unusefull when i input the command "reset" in uboot mode or "reboot" under the system,what should i do?

0 Kudos
Reply
1 Solution
1,257 Views
ufedor
NXP Employee
NXP Employee

Ensure that RESET_REQ_B is properly connected, so that its assertion will generate PORESET_B low pulse having at least 1 ms duration.

View solution in original post

0 Kudos
Reply
2 Replies
1,258 Views
ufedor
NXP Employee
NXP Employee

Ensure that RESET_REQ_B is properly connected, so that its assertion will generate PORESET_B low pulse having at least 1 ms duration.

0 Kudos
Reply
1,257 Views
allan_yi
Contributor I

Thanks a lot ,the problem had been solved,the PORESET_B  low plus only 200ns duration befor.

0 Kudos
Reply