LS1043 platform "reset" can not work

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1043 platform "reset" can not work

ソリューションへジャンプ
1,303件の閲覧回数
allan_yi
Contributor I

we use LS1043,it is unusefull when i input the command "reset" in uboot mode or "reboot" under the system,what should i do?

0 件の賞賛
返信
1 解決策
1,250件の閲覧回数
ufedor
NXP Employee
NXP Employee

Ensure that RESET_REQ_B is properly connected, so that its assertion will generate PORESET_B low pulse having at least 1 ms duration.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,251件の閲覧回数
ufedor
NXP Employee
NXP Employee

Ensure that RESET_REQ_B is properly connected, so that its assertion will generate PORESET_B low pulse having at least 1 ms duration.

0 件の賞賛
返信
1,250件の閲覧回数
allan_yi
Contributor I

Thanks a lot ,the problem had been solved,the PORESET_B  low plus only 200ns duration befor.

0 件の賞賛
返信