The version of the kernel image supplied with the ls1021a-iot is different to the default kernel image built using the LS1021A-IoT Rev B Gateway Linux SDK.
I have built the toolchain, filesystem and a starting application. This run OK with the supplied kernel 3.12.0+ image.
I have built the kernel using the recommend SDK,
>bitbake virtual/kernel
this generates Linux-4.1.30-rt34+g73b5a4eeed04.
the just displays
starting kernel.....
(This kernel image was getting over written by the device tree resulting in a bad crc, I have fixed this)
I am trying to workout the best way to proceed given my limited experience with yocto.
What version of the SDK or how can I modify the configuration to rebuild the 3.12.0+ kernel image version supplied?
Any help appreciated.
The latest SDK for the LS1021a-IOT board is available on the following page:
It is SDK Rev 0.1.
Look at FAQ in NXP SDK 2.0-1703 documentation:
http://www.nxp.com/docs/en/supporting-information/QORIQ-SDK-2.0-IC-REV0.pdf
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------