I am new to SDK based programming for QorIQ Processors. Pls guide me how to proceed after SDK Installation. Any presentation or pdf would be nice to have.
See also the following page:
http://www.freescale.com/infocenter/index.jsp?topic=%2FQORIQSDK%2F3069724.html
I was asking examples of software development in C language in SDK
Take a look on this link: About Yocto. If you want to build your code using Yocto, you have to create recipe for your specific package (google for this king of info), otherwise you can just build your application using specific toolchain or the one included in SDK (Standalone toolchain), then include app in your linux rootfs and run it.
One other way is to use CodeWarrior Linux Project, to create, edit, build, debug your linux user space app.
Adrian
Pls elaborate how to "include app in your linux rootfs and run it".
More broadly, pls tell me the steps of how to port my applications to P2020RDB-PCA board, I mean what commands need to be run and at what location for the cross compilation.
Build SDK toolchain using the following page:
http://www.freescale.com/infocenter/index.jsp?topic=%2FQORIQSDK%2F3069706.html
Use the following command for simple_serial c building:
gcc simple_serial.c --sysroot=/opt/fsl-networking/QorIQ-SDK-V1.7/sysroots/ppce500v2-fsl-linux-gnuspe/ -o simple_serial
See corrected simple_serial.c file in the attachment.
Have a great day,
Pavel
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Please take a look on Welcome to the Linux SDK for QorIQ Processors Infocenter , you'll find useful information.
Adrian