How to access the flash via kernel for T4240?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to access the flash via kernel for T4240?

604 次查看
mvicki93
Contributor I

We had bought a T4240 EVM Board, and we are in need to access the Flash via Kernel ..

Is there any API available to access the flash or Is there any module which is available in Kernel to access the flash memory?

Thanks in Advance..

标记 (1)
0 项奖励
回复
1 回复

554 次查看
Pavel
NXP Employee
NXP Employee

Look at the TN-00-25 document from Micron
about MTD device under Linux:
https://www.micron.com/resource-details/89ac4532-0cae-400d-874c-c2b977d126a5

Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复