I need to recreate a U-Boot that was built with the gcc-4.3.74-eglibc-2.8.74/powerpc-linux-gnu/bin/powerpc-linux-gnu-gcc tool chain but have been unable to find it anywhere.
I found major and minor, but not the build version. I suspect it's custom to the NXP tool suite since the install path was /opt/freescale/usr/local/ for the defunct system I'm trying to rebuild.
Thank you.
Hello Kurt Copley,
This version Toolchain is provided in ISO P1020_P2020RDB_20101101_ltib.iso, I have uploaded this ISO in the following link
https://drive.google.com/open?id=1iS3StsubAI-AumRvEHV1FEHcJnU4yvV2
After installing this ISO and run "./ltib", toolchain gcc-4.3.74-eglibc-2.8.74 is installed in /opt/freescale/usr/local/.
Thanks,
Yiping
The ltib ISO is not available in www.nxp.com.