How to use scatter/gather mem2mem transfer with fsl-qdma driver

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to use scatter/gather mem2mem transfer with fsl-qdma driver

1,871 次查看
basudebdas
Contributor I

Hi, I am developing a driver module on LS1046A processor (and Linux OS) and want to use fsl-qdma driver for dma data transfer from memory to memory. I am looking for some reference/documentation on how to use the fsl-qdma driver for this purpose. Looking at the fsl-qdma source code, I see that the current memcpy call only supports one source buffer and one destination buffer. No scatter/gather list support. I want to transfer from a list of buffers to a memory destination. How shall I use source scatter/gather list with this fsl-qdma driver ?  I dont see DMA_SG option also when requesting a channel. Any pointer or advice will be very much appreciated.

0 项奖励
回复
2 回复数

1,647 次查看
Pavel
NXP Employee
NXP Employee

The SG mode has been removed from kernel dma engine driver.

If you want to use SG mode please use the LSDK branch linux-4.9.

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,647 次查看
gyosunshim
Contributor III

Hi, Pavel Chubakov.

It is a long time ago, but I am facing the same problem, so I will reply with any questions.

I am using LSDK1803, and I read the above and used 4.9 because of SG mode.

Why is SG mode removed in higher versions? Is there a better mod to replace?

Thank you,
Best regards.

Gyosun.

0 项奖励
回复