Can't boot u-boot from bank 5 on T4240

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can't boot u-boot from bank 5 on T4240

1,939 次查看
sergeissakov
Contributor I

We have two T4240QDS systems and are seeing this same behavior on both.

We can copy u-boot from bank 1 to bank 4 and then boot successfully from bank 4.

But when we copy u-boot from bank 1 to bank 5 and try to boot from bank 5, the system sits in reset.
Are there boot parameters or something else that has to change in order to use u-boot in bank 5?


Thanks!

标记 (3)
0 项奖励
回复
7 回复数

1,496 次查看
梦田
Contributor II

Dear Serge Issakov

I need your help.

I have a T4240qds board, too.But when I set u-boot environment variables,I type the wrong information.

Could you help me to check it by typing "printenv" when you boot your board?

My information like this:

bootargs=root=/dev/sda3 rw rootdelay=10 size=30000000 console=ttyS0,115200

bootcmd=ext2load sata 0:3 0x1000000 /boot/uImage; ext2load sata 0:3 0xc00000 /boot/dtb_file;bootm 0x1000000 - c00000

I want to know the correct infomation.

Thank you very much!

     mengtian.

0 项奖励
回复

1,496 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Hello Mengtian,

Please check whether this would help youT4240rds boot from sata ssd.

If your problem remains, please create a new thread in QorIQ processor block, you could continue to discuss.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,496 次查看
梦田
Contributor II

Dear Yiping Wang,

     I just follow your advice to modify my "env" of Board T4240QDS  fromT4240rds boot from sata ssd.

     But I still failed.Like this:


=> setenv bootcmd 'setenv bootargs root=/dev/sda1 rw console=ttyS0,115200;sata init;ext2load sata 0:1 1000000 /boot/uImage;ext2load sata 0:1 c00000 /boot/uImage-t4240qds.dtb;bootm 1000000 - c00000'

=> saveenv

Saving Environment to Flash...

Un-Protected 1 sectors

Erasing Flash...

. done

Erased 1 sectors

Writing to Flash... 9....8....7....69....8....7....6....5....4....3....2....1....done

Protected 1 sectors

=> boot

SATA0 (3 Gbps)

       SATA1 (No RDY)

sata - SATA sub system

Usage:

sata sata init - init SATA sub system

sata info - show available SATA devices

sata device [dev] - show or set current device

sata part [dev] - print partition table

sata read addr blk# cnt

sata write addr blk# cnt

** No partition table - sata 0 **

** No partition table - sata 0 **

WARNING: adjusting available memory to 30000000

Wrong Image Format for bootm command

ERROR: can't get kernel image!

=>

I really can't understand how to do with it,could you help me?

Thanks.

0 项奖励
回复

1,496 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Hello Mengtian,

Have you also followed other steps to format and deploy images into SATA?

Thanks,

Yiping

0 项奖励
回复

1,496 次查看
梦田
Contributor II

Dear Yiping Wang,

     My board is T4240qds rather than T4240rds,I cannot solve the problem now.

     Could you help me to check it by typing "printenv" when you boot  board T4240qds?

Thanks!

0 项奖励
回复

1,496 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Hello Serge,

Please refer to this document http://cache.freescale.com/files/32bit/doc/user_guide/T4240QDSQSG.pdf?fasp=1&WT_TYPE=Users Guides&WT_VENDOR=FREESCALE&WT_FILE_FORMAT=pdf&WT_ASSET=Documentation&fileExt=.pdf

The flash space is further divided into 8 virtual banks. With SW6[1:4] = 0000 the mapping is as follows:

|Bank7 | e8000000 - e8ffffff

|Bank6 | e9000000 - e9ffffff

|Bank5 | ea000000 - eaffffff

|Bank4 | eb000000 - ebffffff

|Bank3 | ec000000 - ecffffff

|Bank2 | ed000000 - edffffff

|Bank1 | ee000000 - eeffffff

|Bank0 | ef000000 - efffffff

The default SW6[1:4] = 0000, u-boot is at 0xEFF40000(bank0), RCW is at 0xE8000000 (bank 7), the alternate u-boot is at 0xEBF40000(bank4), alternate RCW is at 0xEC000000(bank3).

Please make sure you have deployed u-boot image and RCW appropriately, assume your switch setting is also SW6[1:4] = 0000.

u-boot is at 0xEAF4000000(bank5), RCW is 0xEB000000(bank4).

Then change SW6[1:4] to bank 5, and boot the system.

U-boot is always at 0xeff80000.

If your problem remains, please describe your procedure in details.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,496 次查看
梦田
Contributor II

Dear Yiping Wang,

I need your help.

I have a T4240qds board, too.But when I set u-boot environment variables,I type the wrong information.

Could you help me to check it by typing "printenv" when you boot your board?

My information like this:

bootargs=root=/dev/sda3 rw rootdelay=10 size=30000000 console=ttyS0,115200

bootcmd=ext2load sata 0:3 0x1000000 /boot/uImage; ext2load sata 0:3 0xc00000 /boot/dtb_file;bootm 0x1000000 - c00000

I want to know the correct infomation.

Thank you very much!

     mengtian.

0 项奖励
回复