T4240rds boot from sata ssd

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T4240rds boot from sata ssd

751 Views
davidking
Contributor I

What is the procedure to deploy an image to a sata ssd connected to the T4240rds? We have already created the partitions and made the filesystem on the ssd using the T4240 and our image running in ram.

Labels (1)
0 Kudos
1 Reply

501 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello David,

Please refer to the following image deploy procedure.

1. Create partitions and make filesystems.

# fdisk /dev/sdx

# mkfs.ext2 /dev/sdx1

The sdx is sda, sdb, sdc depending your system.

2. Mount the ext2 partition to your system, and copy image QorIQ_SDK_V1.6_E6500_<date>_ROOTFS_Image.tar.gz from prebuilt IMAGE ISO to SATA, then extract it.

# sudo tar -zxvf QorIQ_SDK_V1.6_E6500_<date>_ROOTFS_Image.tar.gz

# rm QorIQ_SDK_V1.6_E6500_<date>_ROOTFS_Image.tar.gz

3. Copy the target Kernel image uImage and dtb files to SATA "boot" folder.

4. Set the environment in u-boot and boot the system.

# setenv bootcmd 'setenv bootargs root=/dev/sda1 rw console=ttyS0,115200;sata init;ext2load sata 0:1 1000000 /boot/uImage;ext2load sata 0:1 c00000 /boot/uImage-<platform>.dtb;bootm 1000000 - c00000'

# boot


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos