Have a great day,
What do you mean as “all the L2 Eth interfaces in the T1040”? Do you mean the T1040 internal Ethernet switch?
This switch has 8 Ethernet ports, which are tri-speed 10/100/1000 Mbps ports. All these ports can be configured for 100 Mbps.
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------