Can all the L2 Eth interfaces in the T1040 be used as 10/100 Mbit or just GigE?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can all the L2 Eth interfaces in the T1040 be used as 10/100 Mbit or just GigE?

453件の閲覧回数
luisroa
Contributor I

Can all the L2 Eth interfaces in the T1040 be used as 10/100 Mbit simultaneously or just GigE?

0 件の賞賛
返信
1 返信

420件の閲覧回数
r8070z
NXP Employee
NXP Employee

Have a great day,

What do you mean as “all the L2 Eth interfaces in the T1040”? Do you mean the T1040 internal Ethernet switch?

This switch has 8 Ethernet ports, which are tri-speed 10/100/1000 Mbps ports. All these ports can be configured for 100 Mbps.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信