About UART operation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About UART operation

691件の閲覧回数
kojimiura
Contributor I
UART2_SIN is pulled down with 10kΩ.
When not using UART2 (DUART registers remain at their initial values)
1. Will it harm my device?
2. Would you like to receive data?
3. Is it possible for the CPU to be interrupted for some reason?
4. Is it okay if the Divisor setting value is zero?
Thank you.
0 件の賞賛
返信
6 返答(返信)

607件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

When not using UART2 , the response for the above-stated queries are as follows:
1. Will it harm my device
No

2. Would you like to receive data?
No

3. Is it possible for the CPU to be interrupted for some reason?
No

4. Is it okay if the Divisor setting value is zero?
Does not matter.

0 件の賞賛
返信

652件の閲覧回数
kojimiura
Contributor I

What do you think after that?

0 件の賞賛
返信

647件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Discussing with the AE team.

0 件の賞賛
返信

551件の閲覧回数
kojimiura
Contributor I

Since the internal clock of UART2 is disabled, Start bit is not detected. Is this understanding correct?

0 件の賞賛
返信

544件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Yes, correct.

0 件の賞賛
返信

541件の閲覧回数
kojimiura
Contributor I
Thank you.
0 件の賞賛
返信