BSC9132 changing eSPI frequency

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

BSC9132 changing eSPI frequency

ソリューションへジャンプ
1,568件の閲覧回数
brianarellano
Contributor I

HI,

We have a custom BSC9132 board and we are getting issues on SPI2 bus timing. Is it possible to adjust the SPI2 frequency after booting linux? Say, adjust the READ transaction to 10Mhz and WRITE to 20Mhz.

Thanks.

Brian

ラベル(1)
0 件の賞賛
返信
1 解決策
1,377件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

The eSPI controller has 4 chip selects and clock modulus and clock pre-divider is configurable per-chip select. This means you can have individual clock settings per chip select, and also I do not see anything wrong if you will change clock settings before every SPI transaction.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,378件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

The eSPI controller has 4 chip selects and clock modulus and clock pre-divider is configurable per-chip select. This means you can have individual clock settings per chip select, and also I do not see anything wrong if you will change clock settings before every SPI transaction.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信