Getting started with B4860QDS Board 'out of the box'

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Getting started with B4860QDS Board 'out of the box'

1,033 Views
markdoherty
Contributor I

SN SCH-27234 Rev C1 700-27234 Rev H

I cannot get the USB eCWTAP to work

LD9 &10 are green

When power connected and not started L1 and L2 are OFF. When started L1 and L2 are still OFF, LD8 is green.

ccs/drivers/usb seems to uninstall / install but jungo/detect reports that is is not installed

Further,

I have installed the 1.7 SDK VDI on windows VirtualBox.

Where is the USDPAA classifier demo located?

Labels (1)
0 Kudos
Reply
1 Reply

776 Views
lunminliang
NXP Employee
NXP Employee

Hi,

For the first question, you could reinstall driver following steps in readme.txt, which is in C:\Freescale\CW_SC_3900FP_v10.8.1\SC\ccs\drivers\usb.

What target are you trying to connect?

There is post containing some discussion about this, you may refer to

Getting started with B4860QDS Board 'out of the box'

For the second one, see git2_git.freescale.com.ppc.sdk.usdpaa.git.tar.gz under below path in you VirtualBox Guest:

~/SDK/QorIQ-SDK-V1.7-20141218-yocto/sources

or

/home/freescale/SDK/QorIQ-SDK-V1.7-20141218-yocto/sources


Have a great day,
Lunmin

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply