iMX8qm - Enable USB 2.0 otg1 port to download image from UUU

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX8qm - Enable USB 2.0 otg1 port to download image from UUU

Jump to solution
4,600 Views
sig0912
Contributor III

Hi everyone,

We are using a custom board based on imx8qm mek devkit. We removed the USB type C, instead we use a USB micro-B. The USB is connected to the USBOH block as shown in the picture below.

Ingrid_0-1635236722097.png

We would like to download the bootloader via USB to a SPI nor flash memory using uuu tool.

Unfortunately after loading the boot image the imx8 doesn't come up as a new device under the device manager as it does on the devkit.. It supposed to come up as VID=0x0525, PID=0xa4a5 as defined in the defconfig

To boot the image from uuu we use: SDPS: boot -f flash.bin -skipfhdr.

Ingrid_1-1635236946301.png

Ingrid_2-1635237189410.png

The imx8 is properly booted but no USB device is found. We have followed some other posts about the same problem but with no success. So can you explain in detail how to use USB 2.0 usbotg1 instead of Type C usbotg2 for downloading image and what modification need to be done in defconfig, dts...? We have attached our dts and config files.

We are using uboot-imx branch imx_5.4.24_er3 and code has been modified as followed:

- imx8qm_mek_defconfig

diff --git a/configs/imx8qm_mek_defconfig b/configs/imx8qm_mek_defconfig
index dbe71b0..3ac302d 100644
--- a/configs/imx8qm_mek_defconfig
+++ b/configs/imx8qm_mek_defconfig
@@ -114,29 +114,29 @@ CONFIG_SF_DEFAULT_CS=0
CONFIG_SF_DEFAULT_SPEED=40000000
CONFIG_SF_DEFAULT_MODE=0

-CONFIG_USB_XHCI_HCD=y
-CONFIG_USB_XHCI_IMX8=y
+CONFIG_USB_XHCI_HCD=n
+CONFIG_USB_XHCI_IMX8=n
CONFIG_DM_USB=y
CONFIG_DM_USB_GADGET=y
CONFIG_SPL_DM_USB_GADGET=y
CONFIG_USB=y
-CONFIG_USB_TCPC=y
+CONFIG_USB_TCPC=n
CONFIG_USB_GADGET=y
CONFIG_CI_UDC=y
CONFIG_USB_GADGET_DOWNLOAD=y
CONFIG_USB_GADGET_MANUFACTURER="FSL"
CONFIG_USB_GADGET_VENDOR_NUM=0x0525
CONFIG_USB_GADGET_PRODUCT_NUM=0xa4a5
-CONFIG_USB_CDNS3=y
-CONFIG_USB_CDNS3_GADGET=y
+CONFIG_USB_CDNS3=n
+CONFIG_USB_CDNS3_GADGET=n
CONFIG_USB_GADGET_DUALSPEED=y
-CONFIG_CDNS3_USB_PHY=y
+CONFIG_CDNS3_USB_PHY=n
CONFIG_PHY=y
CONFIG_SPL_PHY=y

CONFIG_SPL_USB_GADGET=y
CONFIG_SPL_USB_SDP_SUPPORT=y
-CONFIG_SPL_SDP_USB_DEV=1
+CONFIG_SPL_SDP_USB_DEV=0
CONFIG_SDP_LOADADDR=0x80400000

CONFIG_FASTBOOT=y
@@ -147,7 +147,7 @@ CONFIG_FASTBOOT_UUU_SUPPORT=y
CONFIG_FASTBOOT_BUF_ADDR=0x82800000
CONFIG_FASTBOOT_BUF_SIZE=0x40000000
CONFIG_FASTBOOT_FLASH=y
-CONFIG_FASTBOOT_USB_DEV=1
+CONFIG_FASTBOOT_USB_DEV=0

- fsl-imx8qm-mek.dts

typec_ptn5110 node for type c is commented out

&usbotg1 {
  status = "okay";
}

&usbotg3 {
  status = "disabled";
}

- fsl-imx8qm-mek-u-boot.dtsi

All nodes related to USB3 (usbh3, usbotg3, usbphynop1) have been commented out. Only usbotg1 is kept.

Can you explain as well which code should be executed to initialize the USB device? There is the function board_usb_init that should be called in imx8qm_mek.c, and surprisingly there is no code executed when index is different than 1. And it seems that at this stage of the boot this function is not called at all anyway. In our case index is 0 because we use USB2 otg1. Is there other code to check for this usb initialization?

Ingrid_3-1635239294342.png

Can someone please help with this, we are stuck in our development due to this problem.

Thank you for you help
Best Regards

Labels (1)
Tags (4)
0 Kudos
Reply
1 Solution
4,595 Views
sig0912
Contributor III

Problem solved, USB_OTG1_ID needed to be pulled up to High. 
This link was a great help: https://community.nxp.com/t5/i-MX-Processors/MX6ULL-OTG-not-working/m-p/1034875

 

View solution in original post

0 Kudos
Reply
1 Reply
4,596 Views
sig0912
Contributor III

Problem solved, USB_OTG1_ID needed to be pulled up to High. 
This link was a great help: https://community.nxp.com/t5/i-MX-Processors/MX6ULL-OTG-not-working/m-p/1034875

 

0 Kudos
Reply