How can I get a package for the MK60DN512ZCAB (120 WCLSP) ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How can I get a package for the MK60DN512ZCAB (120 WCLSP) ?

494 次查看
johnwoods
Contributor I

I don't see the 120 WCLSP package available. Is there a way to create a custom package or can I download one somewhere?

标记 (5)
0 项奖励
回复
1 回复

417 次查看
BlackNight
NXP Employee
NXP Employee

Yes, that package is not listed. However, from a software perspective what counts are the pins which are routed to the package (independent which packages is used). So from this perspective, the BGA (ball grid array) package is what you could use instead?

0 项奖励
回复