Traces under Isolated Gate Driver

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Traces under Isolated Gate Driver

Jump to solution
2,322 Views
travisalexander
NXP Employee
NXP Employee

Hey Travis,

Could you advise on this question?

 

I've seen that your competitors will state in their datasheets that no traces or planes should be placed underneath the isolation area. Is this also the case for the NXP part?

 

 

 

Jack Jamieson

M: (419) 261-5225

 

Labels (1)
0 Kudos
Reply
1 Solution
2,318 Views
travisalexander
NXP Employee
NXP Employee

Hi Jack,

Yes this is the case--no traces under the IC.

The reason you can't have traces under the gate driver is to meet creepage and clearance isolation requirements separating the HV gate from the LV MCU side.

We put this information in the GD3100 app note (AN12357, section 9.1).

Regards,

Travis

View solution in original post

0 Kudos
Reply
1 Reply
2,319 Views
travisalexander
NXP Employee
NXP Employee

Hi Jack,

Yes this is the case--no traces under the IC.

The reason you can't have traces under the gate driver is to meet creepage and clearance isolation requirements separating the HV gate from the LV MCU side.

We put this information in the GD3100 app note (AN12357, section 9.1).

Regards,

Travis

0 Kudos
Reply