p2020是否支持 ELBC与DDR之间DMA传输

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

p2020是否支持 ELBC与DDR之间DMA传输

1,149件の閲覧回数
Jaygao
Contributor I

p2020_dma.PNG

0 件の賞賛
返信
2 返答(返信)

1,103件の閲覧回数
June_Lu
NXP TechSupport
NXP TechSupport

13.4.2 DMA transfer interfaces
The DMA can be used to achieve data transfers across the entire memory map.
Note that a single DMA transfer in any of the direct or chaining modes must not cross a
16 GB (34-bit) address boundary.

0 件の賞賛
返信

925件の閲覧回数
Jaygao
Contributor I

is the external request need for the DMA transcation between e LBC and ddr?

0 件の賞賛
返信