mpc8379 vsc7385

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mpc8379 vsc7385

564 Views
jfsong1
Contributor I

hello, where can I find the source code of VSC7385 in the mpc8379 BSP which contains vsc2bin ?  I am wrong in using the switch led pin functions which indicate 1000Mbps and Tx. I want to reassign the led pin definitions through changing the source code of VSC7385 . If possible, any other simple methods will be preferred except changing source code. Thank you .

0 Kudos
2 Replies

436 Views
ufedor
NXP Employee
NXP Employee

VSC7385 is not an NXP product. We neither develop, nor distribute source codes for it. The firmware binary included in the BSP is a standard unmanaged switch firmware that was available from Vitesse at the moment of the BSP development.

0 Kudos

436 Views
jfsong1
Contributor I

Thanks  a lot.

0 Kudos