Reset sequence is not working in T1014NXEPQA

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Reset sequence is not working in T1014NXEPQA

1,014 Views
EC146552
Contributor I

Asleep signal is always coming low while starting of reset sequence of T1014NXWPQA.

First, we are providing POR and then T1014 is driving HRST signal low but when POR is high then after 3ms HRST_REQ signal is coming from processor and then againg we are providing POR low and this sequence is repeating again and again.

and  throughout this ASLEEP is low.

how to generate reset sequence for T1014?

please help

0 Kudos
Reply
1 Reply

890 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to section# 4.7.1 and figure# 4-1 of the T1024RM and let me know from which part of the sequence is the system going wrong.

 

Also, share the complete debug logs and if possible the schematic of the design.

0 Kudos
Reply