Reprogramming DDR controller on PowerQUICC III

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Reprogramming DDR controller on PowerQUICC III

864 次查看
ConfusedInOR
Contributor I

Is it possible to reprogram the DDR controller on PowerQUICC III more than once after power-up?  Our system uses two bootROM (once factory installed, one field-upgradable) and the DDR is programmed in both (not necessarily with the same settings).  Is there a different program sequence needed the second time though?  Thanks!

0 项奖励
回复
0 回复数