MPC8533EVJANGA

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MPC8533EVJANGA

跳至解决方案
710 次查看
meo081101
Contributor II

Hello,

Can I replace a MPC8533VTALF by a MPC8533EVJANGA?

Can you give me document that shows diffirent between MPC8533VTALF and MPC8533EVJANGA?

Thank you!

Kean

1 解答
626 次查看
r8070z
NXP Employee
NXP Employee


Have a great day,

Please see section 22.2 “Nomenclature of Parts Fully Addressed by this Document” in the data sheet

https://www.nxp.com/docs/en/data-sheet/MPC8533EEC.pdf

Using table Table Device Nomenclature you can easily see the differences. Notice for migration from VT device to VJ device there is PCN “Device Migration from Leaded Wafer Bumps to Lead-Free Wafer Bumps”

https://www.nxp.com/docs/en/product-change-notice/PCN16365.htm

For each MPC8533 device you can get details on the nxp site. For example for the MPC8533EVJANGA see page

https://www.nxp.com/part/MPC8533EVJANGA

Because these devices have different revision  you may need to check the MPC8533 errata, some issues have been fixed on new revision. Unfortunately it is not public document (requires for NDA).

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

2 回复数
627 次查看
r8070z
NXP Employee
NXP Employee


Have a great day,

Please see section 22.2 “Nomenclature of Parts Fully Addressed by this Document” in the data sheet

https://www.nxp.com/docs/en/data-sheet/MPC8533EEC.pdf

Using table Table Device Nomenclature you can easily see the differences. Notice for migration from VT device to VJ device there is PCN “Device Migration from Leaded Wafer Bumps to Lead-Free Wafer Bumps”

https://www.nxp.com/docs/en/product-change-notice/PCN16365.htm

For each MPC8533 device you can get details on the nxp site. For example for the MPC8533EVJANGA see page

https://www.nxp.com/part/MPC8533EVJANGA

Because these devices have different revision  you may need to check the MPC8533 errata, some issues have been fixed on new revision. Unfortunately it is not public document (requires for NDA).

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

626 次查看
meo081101
Contributor II

Have a nice day,

Thank you for your helpful answer!

0 项奖励