MPC8358 DDR2 ECC Registered

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC8358 DDR2 ECC Registered

Jump to solution
1,151 Views
Amit24
Contributor I

Hi we have used  MPC8358 in our design a 5 year ago. Now, we are facing a problem shortage of DDR2 SDRAM ECC registered buffered.So Anyone cal able to tell me, Can we replace or design a new board with Standard SODIMM unbuffered DDR2  or with discrete chips.

Regrads

Amit Kumar

0 Kudos
1 Solution
1,138 Views
r8070z
NXP Employee
NXP Employee

Yes you can.
The MPC8360 reference manual says: The fully programmable DDR SDRAM controller supports most JEDEC standard ×8, ×16, or ×32 DDR2 and DDR memories available. In addition, unbuffered and registered DIMMs are supported. However, mixing different memory types or unbuffered and registered DIMMs in the same system is not supported. It also provides supported configurations

r8070z_1-1623071679923.png

 

View solution in original post

0 Kudos
5 Replies
1,079 Views
Amit24
Contributor I

Hi,

Can i use 240 pin memory module with this ? if anyone have some resources , please share .

 

Thanks

Amit 

 

0 Kudos
1,130 Views
Amit24
Contributor I

Thanks for feedbck,Do you have reference circuit interfacing SODIMM or dicrete SDRAM chips?

Please share if you have.

Regards

Amit

0 Kudos
1,139 Views
r8070z
NXP Employee
NXP Employee

Yes you can.
The MPC8360 reference manual says: The fully programmable DDR SDRAM controller supports most JEDEC standard ×8, ×16, or ×32 DDR2 and DDR memories available. In addition, unbuffered and registered DIMMs are supported. However, mixing different memory types or unbuffered and registered DIMMs in the same system is not supported. It also provides supported configurations

r8070z_1-1623071679923.png

 

0 Kudos
1,133 Views
Amit24
Contributor I
 
0 Kudos
1,121 Views
r8070z
NXP Employee
NXP Employee

Check MPC8360EMDS: MPC8360EA Modular Development System page

https://www.nxp.com/design/qoriq-developer-resources/mpc8360ea-modular-development-system:MPC8360EMD...

I provides some design resources, including schematics of board with DDR2 SODIMM

https://www.nxp.com/downloads/en/schematics/MPC8360EAMDSSCH.pdf

0 Kudos