MPC8358 DDR2 ECC Registered

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MPC8358 DDR2 ECC Registered

跳至解决方案
2,306 次查看
Amit24
Contributor I

Hi we have used  MPC8358 in our design a 5 year ago. Now, we are facing a problem shortage of DDR2 SDRAM ECC registered buffered.So Anyone cal able to tell me, Can we replace or design a new board with Standard SODIMM unbuffered DDR2  or with discrete chips.

Regrads

Amit Kumar

0 项奖励
回复
1 解答
2,293 次查看
r8070z
NXP Employee
NXP Employee

Yes you can.
The MPC8360 reference manual says: The fully programmable DDR SDRAM controller supports most JEDEC standard ×8, ×16, or ×32 DDR2 and DDR memories available. In addition, unbuffered and registered DIMMs are supported. However, mixing different memory types or unbuffered and registered DIMMs in the same system is not supported. It also provides supported configurations

r8070z_1-1623071679923.png

 

在原帖中查看解决方案

0 项奖励
回复
5 回复数
2,234 次查看
Amit24
Contributor I

Hi,

Can i use 240 pin memory module with this ? if anyone have some resources , please share .

 

Thanks

Amit 

 

0 项奖励
回复
2,285 次查看
Amit24
Contributor I

Thanks for feedbck,Do you have reference circuit interfacing SODIMM or dicrete SDRAM chips?

Please share if you have.

Regards

Amit

0 项奖励
回复
2,294 次查看
r8070z
NXP Employee
NXP Employee

Yes you can.
The MPC8360 reference manual says: The fully programmable DDR SDRAM controller supports most JEDEC standard ×8, ×16, or ×32 DDR2 and DDR memories available. In addition, unbuffered and registered DIMMs are supported. However, mixing different memory types or unbuffered and registered DIMMs in the same system is not supported. It also provides supported configurations

r8070z_1-1623071679923.png

 

0 项奖励
回复
2,288 次查看
Amit24
Contributor I
 
0 项奖励
回复
2,276 次查看
r8070z
NXP Employee
NXP Employee

Check MPC8360EMDS: MPC8360EA Modular Development System page

https://www.nxp.com/design/qoriq-developer-resources/mpc8360ea-modular-development-system:MPC8360EMD...

I provides some design resources, including schematics of board with DDR2 SODIMM

https://www.nxp.com/downloads/en/schematics/MPC8360EAMDSSCH.pdf

0 项奖励
回复