MPC8308: RGMII (eTSEC1) at 3.3V? or only 2.5V?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC8308: RGMII (eTSEC1) at 3.3V? or only 2.5V?

1,249件の閲覧回数
jmaccedian
Contributor I

We're using the MPC8308. There is a confusion between the datasheet and some schematic about the supply for the eTSEC1 in RGMII mode. Can we connect the eTSEC1 at 3.3V in RGMII mode? or it's only 2.5V? LVDD1 = NVDDC = TSEC1 = ? in RGMII mode


JMAccedian

ラベル(1)
0 件の賞賛
返信
1 返信

632件の閲覧回数
andrei_skok
NXP Employee
NXP Employee

According to the MPC8308 Datasheet:

"The RGMII interface is defined for 2.5 V, while the MII interface can be operated at 3.3 V"

If you use eTSEC1 in RGMII mode you should connect LVDD1 (NVDDC) to 2,5V.

0 件の賞賛
返信