CodeWarrior8.8 for CodeWarrior TAP,MPC8309

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWarrior8.8 for CodeWarrior TAP,MPC8309

Jump to solution
1,617 Views
tom3721
Contributor I

The software I used to use was Code Warrior8.8, and the emulator I used was CodeWarrior USB TAP. Now I have purchased CodeWarrior TAP, but this emulator cannot be correctly recognized in Code Warrior 8.8. Is there any additional program to correct this?

0 Kudos
1 Solution
1,612 Views
yipingwang
NXP TechSupport
NXP TechSupport

You need to apply Patch 8.8.6 to update CodeWarrior CCS USB driver to support CodeWarrior TAP.

Please login https://www.nxp.com, then download Patch 8.8.6 from "My NXP Account->Software Licensing and Support->View accounts->NXP Software->CodeWarrior Networked Suite - Specialist Level -> 8.8 CodeWarrior DS for Power Architecture, Professional Edition (Windows Hosted) WIN->Software Patch: CW PA v8.8.6 Windows - Patch.

View solution in original post

0 Kudos
4 Replies
1,239 Views
laohu113
Contributor I

Hello, I have the same situation as you, but after I installed the patch, the result is the same as before, do you remember there are some special steps?

0 Kudos
1,232 Views
tom3721
Contributor I

我安装了补丁后就能正常使用了,没有碰到其它问题。

0 Kudos
1,613 Views
yipingwang
NXP TechSupport
NXP TechSupport

You need to apply Patch 8.8.6 to update CodeWarrior CCS USB driver to support CodeWarrior TAP.

Please login https://www.nxp.com, then download Patch 8.8.6 from "My NXP Account->Software Licensing and Support->View accounts->NXP Software->CodeWarrior Networked Suite - Specialist Level -> 8.8 CodeWarrior DS for Power Architecture, Professional Edition (Windows Hosted) WIN->Software Patch: CW PA v8.8.6 Windows - Patch.

0 Kudos
1,609 Views
tom3721
Contributor I

Thank you very much. The problem has been solved after installing the patch.

0 Kudos