CodeWarrior8.8 for CodeWarrior TAP,MPC8309

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

CodeWarrior8.8 for CodeWarrior TAP,MPC8309

跳至解决方案
1,791 次查看
tom3721
Contributor I

The software I used to use was Code Warrior8.8, and the emulator I used was CodeWarrior USB TAP. Now I have purchased CodeWarrior TAP, but this emulator cannot be correctly recognized in Code Warrior 8.8. Is there any additional program to correct this?

0 项奖励
回复
1 解答
1,786 次查看
yipingwang
NXP TechSupport
NXP TechSupport

You need to apply Patch 8.8.6 to update CodeWarrior CCS USB driver to support CodeWarrior TAP.

Please login https://www.nxp.com, then download Patch 8.8.6 from "My NXP Account->Software Licensing and Support->View accounts->NXP Software->CodeWarrior Networked Suite - Specialist Level -> 8.8 CodeWarrior DS for Power Architecture, Professional Edition (Windows Hosted) WIN->Software Patch: CW PA v8.8.6 Windows - Patch.

在原帖中查看解决方案

0 项奖励
回复
4 回复数
1,413 次查看
laohu113
Contributor I

Hello, I have the same situation as you, but after I installed the patch, the result is the same as before, do you remember there are some special steps?

0 项奖励
回复
1,406 次查看
tom3721
Contributor I

我安装了补丁后就能正常使用了,没有碰到其它问题。

0 项奖励
回复
1,787 次查看
yipingwang
NXP TechSupport
NXP TechSupport

You need to apply Patch 8.8.6 to update CodeWarrior CCS USB driver to support CodeWarrior TAP.

Please login https://www.nxp.com, then download Patch 8.8.6 from "My NXP Account->Software Licensing and Support->View accounts->NXP Software->CodeWarrior Networked Suite - Specialist Level -> 8.8 CodeWarrior DS for Power Architecture, Professional Edition (Windows Hosted) WIN->Software Patch: CW PA v8.8.6 Windows - Patch.

0 项奖励
回复
1,783 次查看
tom3721
Contributor I

Thank you very much. The problem has been solved after installing the patch.

0 项奖励
回复