I am trying to compare SBC chips UJA1167 and UJA1169. I want to use the UJA1167 SBC. The problem is I cannot find a document or tool that does this comparison. I see there is a driver already developed in the cookbok for s32k144, which is the sbc_uja1169.h . My guess is that these two chips are very similar but it would be very helpful a document or a tool to compare them and know which registers and fields change between them.
Hi Juan,
I would recommend taking a closer look at the attached AH1306. Section 12.6 describes software flow differences between UJA1164/7/8/9 SBCs.
Please create a standard ticket if you are interested in the UJA1167 example project which demonstrates how to:
- Program the UJA1167 MTP
- Initialize the UJA1167
- Trigger the watchdog
- Change operation modes
- Handle events etc.
Best regards,
Tomas