re-enable SYNCIN pin on PF8200

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

re-enable SYNCIN pin on PF8200

ソリューションへジャンプ
965件の閲覧回数
K_Steinhammer
Contributor III

In a custom i.MX8QM board, we are using two PF8200 PMICs (MC33PF8200ESES and MC33PF8200DBES) in combination with several other switching power supplies. In order to optimize EMI behavior, we want to synchronize all PSU to a common reference clock.

For the PF8200 I understood this could be done by applying the reference clock to the SYNCIN pin - which, according to the OTP programming reports, is disabled in both variants during power up because of the OTP configuration.

(a) Do I have the right understanding here?

(b) If the answer on (a) is yes, is there a way to enable SYNCIN again during runtime via I2C?

(c) If the answer on (b) is yes, how do I re-enable SYNCIN?

 

Thanks

タグ(1)
0 件の賞賛
1 解決策
962件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Klaus,

For both the MC33PF8200ESES and MC33PF8200DBES the external clock synchronization is disabled (OTP_SYNCIN_EN = 0) and there is no way to enable this function during runtime via I2C.

Best regards,

Tomas

元の投稿で解決策を見る

1 返信
963件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Klaus,

For both the MC33PF8200ESES and MC33PF8200DBES the external clock synchronization is disabled (OTP_SYNCIN_EN = 0) and there is no way to enable this function during runtime via I2C.

Best regards,

Tomas