re-enable SYNCIN pin on PF8200

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

re-enable SYNCIN pin on PF8200

Jump to solution
1,200 Views
K_Steinhammer
Contributor III

In a custom i.MX8QM board, we are using two PF8200 PMICs (MC33PF8200ESES and MC33PF8200DBES) in combination with several other switching power supplies. In order to optimize EMI behavior, we want to synchronize all PSU to a common reference clock.

For the PF8200 I understood this could be done by applying the reference clock to the SYNCIN pin - which, according to the OTP programming reports, is disabled in both variants during power up because of the OTP configuration.

(a) Do I have the right understanding here?

(b) If the answer on (a) is yes, is there a way to enable SYNCIN again during runtime via I2C?

(c) If the answer on (b) is yes, how do I re-enable SYNCIN?

 

Thanks

Tags (1)
0 Kudos
Reply
1 Solution
1,197 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Klaus,

For both the MC33PF8200ESES and MC33PF8200DBES the external clock synchronization is disabled (OTP_SYNCIN_EN = 0) and there is no way to enable this function during runtime via I2C.

Best regards,

Tomas

View solution in original post

1 Reply
1,198 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Klaus,

For both the MC33PF8200ESES and MC33PF8200DBES the external clock synchronization is disabled (OTP_SYNCIN_EN = 0) and there is no way to enable this function during runtime via I2C.

Best regards,

Tomas