TEA2208

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 
1,238 Views
alessandrocunha
Contributor I

Any usage example available for this TEA2208 that I can share with my customers?

0 Kudos
1 Solution
1,228 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Alessandro,

 

The TEA2208T is intended for power supplies with a boost-type power-factor controller as a first stage. The second stage can be a resonant controller, a flyback controller, or any other controller topology. It can be used in all power supplies requiring high efficiency:

  • (Notebook) Adapters
  • Power supplies for desktop and all-in-one PCs
  • Power supplies for gaming consoles
  • Power supplies for UHD LED / OLED televisions
  • Power supplies for servers / 5G

 

Currently we offer the TEA2208DB1576 demo board. In the UM11348 (Fig. 5) you can see this board mounted on the TEA2016DB1519 240W resonant adapter board.

 

Best regards,

Tomas

View solution in original post

2 Replies
1,229 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Alessandro,

 

The TEA2208T is intended for power supplies with a boost-type power-factor controller as a first stage. The second stage can be a resonant controller, a flyback controller, or any other controller topology. It can be used in all power supplies requiring high efficiency:

  • (Notebook) Adapters
  • Power supplies for desktop and all-in-one PCs
  • Power supplies for gaming consoles
  • Power supplies for UHD LED / OLED televisions
  • Power supplies for servers / 5G

 

Currently we offer the TEA2208DB1576 demo board. In the UM11348 (Fig. 5) you can see this board mounted on the TEA2016DB1519 240W resonant adapter board.

 

Best regards,

Tomas

1,216 Views
alessandrocunha
Contributor I

Thank you @TomasVaverka !

 

Exactly this that I need!

 

Regards

0 Kudos