PF8100 VSNVS output Impossible Voltage

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PF8100 VSNVS output Impossible Voltage

12,581 次查看
chinachuli
Contributor II

when i modify "i.MX8QXP MEK schematic" to my own imx8qxp board, see attachment,i find VSNVS pin output at 5v, in datesheet VSNVS max output voltage is 3.3v. i do not know where is wrong, thanks for give me some suggesstion!

pastedImage_1.png

我在用官方IMX8QXP修改至自己的核心板,主要是简化了不必要的接口电路,原理图见附件,但我板子做回来测量发现VSNVS的输出有5V,而数据手册上最高电压为3.3V,找了很大时间未找出原因,所以求助论坛,非常感谢!

标签 (2)
标记 (1)
0 项奖励
回复
8 回复数

12,185 次查看
chinachuli
Contributor II

Simplify board to only have pmic part, schematic see attachment,VSNVS also output 5V, Where is wrong

0 项奖励
回复

12,186 次查看
guoweisun
NXP TechSupport
NXP TechSupport

Hi,

Do you connect with light load on this VSNVS output then see the actual output?

0 项奖励
回复

12,185 次查看
chinachuli
Contributor II

when VSNVS load 1k ,the actual output still is 5V 

0 项奖励
回复

12,185 次查看
guoweisun
NXP TechSupport
NXP TechSupport

Hi

Do you mind have a phone call with me?

Or give your phone number!

0 项奖励
回复

12,186 次查看
chinachuli
Contributor II

孙工:

我想用二层板做一块pf8100的测试板,原理图见附件。

在 2018-12-04 13:17:36,"褚立" <chinachuli@163.com> 写道:

HI:

我的电话:18158182825 褚立 非常感谢!

0 项奖励
回复

12,186 次查看
guoweisun
NXP TechSupport
NXP TechSupport

Hi

可以这样做,或者你能预留一个Li-ion battery的位置方便调试,拉出来IIC的信号出来。

0 项奖励
回复

12,185 次查看
chinachuli
Contributor II

HI:

我的电话:18158182825 褚立 非常感谢!

0 项奖励
回复

12,185 次查看
guoweisun
NXP TechSupport
NXP TechSupport

Hi,

This should not PMIC's issue,you can disconnect VSNVS with your system only test VSNVS output to check PMIC good or not.

0 项奖励
回复