I am seeing behaviour on the LOADSW_CTRL register (0x2A) of PCA9450CHNY that doesn't match the documentation. In table 64 of the datasheet is shows the reset state of the register is 0x85, which allows SW_EN to control the state of the load switch. We are seeing that devices actually power up with a default state of 0x84, which sets the load switch to "Always off". Is this expected?
解決済! 解決策の投稿を見る。
Hello Omar,
Indeed, the default value of the LOADSW_CTRL register should be 0x85.
In this case, I assume the device is detecting a short circuit current based on the SW_SC bit as follow:
As a test, could you please set this bit (SW_SC) to 1? If the device restarts in 100ms, indeed, the switch is detecting a short circuit.
Please let me know the results.
Regards,
David
Hi David,
Many thanks for your suggestion. When I change SW_SC to 1 I can see that the power is up after 100ms, confirming that a short circuit is being detected. This appears to be in-rush and so we will amend the design to prevent this from happening.
Hello Omar,
Indeed, the default value of the LOADSW_CTRL register should be 0x85.
In this case, I assume the device is detecting a short circuit current based on the SW_SC bit as follow:
As a test, could you please set this bit (SW_SC) to 1? If the device restarts in 100ms, indeed, the switch is detecting a short circuit.
Please let me know the results.
Regards,
David