Can you program PCA9632 with non-default settings?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Can you program PCA9632 with non-default settings?

跳至解决方案
1,061 次查看
CoryP
Contributor I

Hi, I need a PWM controller to control the brightness of a set of LEDs and I'm considering using the PCA9632. This is perfect for my needs except for one thing.

The power-on configuration appears to be SLEEP with 0% duty cycle on all outputs. I'd prefer if it could power on directly into OSC on, with 50% duty cycle on one of the pins. From my understanding of the datasheet, this must be programmed on every power-on.

Is there a way to configure the power-on defaults so that I don't have to create a script to send 3-4 of the same I2C commands on every power-up? This would complicate things because I would need my microcontroller to do this while it powers up at the same time as this chip.

Thanks,

Cory

0 项奖励
回复
1 解答
1,042 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Cory,

Thank you for considering the PCA9632 for your application.

As you correctly stated, the oscillator is off (low power mode) and duty cycles in PWMx registers set to 0% by default.

Unfortunately, the PCA9632 does not allow to pre-configure the default settings in OTP or similar, it needs to be set every time the power is turned on.

Regards,

Tomas

在原帖中查看解决方案

0 项奖励
回复
5 回复数
1,043 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Cory,

Thank you for considering the PCA9632 for your application.

As you correctly stated, the oscillator is off (low power mode) and duty cycles in PWMx registers set to 0% by default.

Unfortunately, the PCA9632 does not allow to pre-configure the default settings in OTP or similar, it needs to be set every time the power is turned on.

Regards,

Tomas

0 项奖励
回复
1,037 次查看
CoryP
Contributor I

Ah I see, thank you for clarifying.

0 项奖励
回复
1,036 次查看
CoryP
Contributor I

Oh wait, one more question: Do you know if NXP has any similar product in the same family that does allow this?

0 项奖励
回复
1,030 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Unfortunately, currently not.

0 项奖励
回复
1,026 次查看
CoryP
Contributor I

Ok I see. Thank you again for the information!

0 项奖励
回复