I am having a custom board based on P1022 processor, I wanted to update the kernel to 4.1.8(extracted from QorIQ2.0) from earlier 3.12.37 (extracted from BSP QorIQ1.8) . I have extracted the kernel source of QorIq2.0 and compiled the same kernel using p1022 toolchain. I have successfully generated the kernel image but when i try to load the kernel in my board it fails to load throwing the following exception.
Device: FSL_SDHC
Manufacturer ID: fe
OEM: 14e
Name: MMC04
Tran Speed: 52000000
Rd Block Len: 512
MMC version 4.41
High Capacity: Yes
Capacity: 3.5 GiB
Bus Width: 4-bit
Erase Group Size: 512 KiB
HC WP Group Size: 4 MiB
User Capacity: 3.5 GiB
Boot Capacity: 16 MiB ENH
RPMB Capacity: 128 KiB ENH
12566 bytes read in 112 ms (109.4 KiB/s)
4320640 bytes read in 320 ms (12.9 MiB/s)
WARNING: adjusting available memory to 30000000
## Booting kernel from Legacy Image at 01000000 ...
Image Name: Linux-4.1.8-rt8
Image Type: PowerPC Linux Kernel Image (gzip compressed)
Data Size: 4320576 Bytes = 4.1 MiB
Load Address: 00000000
Entry Point: 00000000
Verifying Checksum ... OK
## Flattened Device Tree blob at 03000000
Booting using the fdt blob at 0x3000000
Uncompressing Kernel Image ... OK
Loading Device Tree to 03ff9000, end 03fff115 ... OK
Note: The same earlier kernel 3.13 when again loaded into the above board works properly and boots the linux.
已解决! 转到解答。
Hello Hemwant Rawat,
I verified your uImage file, encountered same problem as you.
There is problem with uImage which you built.
You could refer to the following procedure to build Linux Kernel image.
Please download SDK image ISO for e500v2, then install Toolchain for e500v2, and execute the following command.
$ source /opt/fsl-qoriq/2.0/environment-setup-ppce500v2-fsl-linux-gnuspe
$ cp arch/powerpc/configs/mpc85xx_defconfig .config
$ make ARCH=powerpc menuconfig
$ unset LDFLAGS
$ make uImage CC="powerpc-fsl-linux-gnuspe-gcc --sysroot=/opt/fsl-qoriq/2.0/sysroots/ppce500v2-fsl-linux-gnuspe"
Thanks,
Yiping
Hello Hemwant Rawat,
Please try whether the attached uImage can work on your target board, which I got from SDK 2.0 e500v2 pre-built image ISO.
Would you please provide your uImage and dtb file? I will verify them on my demo board.
Thanks,
Yiping
Hello Hemwant Rawat,
I verified your uImage file, encountered same problem as you.
There is problem with uImage which you built.
You could refer to the following procedure to build Linux Kernel image.
Please download SDK image ISO for e500v2, then install Toolchain for e500v2, and execute the following command.
$ source /opt/fsl-qoriq/2.0/environment-setup-ppce500v2-fsl-linux-gnuspe
$ cp arch/powerpc/configs/mpc85xx_defconfig .config
$ make ARCH=powerpc menuconfig
$ unset LDFLAGS
$ make uImage CC="powerpc-fsl-linux-gnuspe-gcc --sysroot=/opt/fsl-qoriq/2.0/sysroots/ppce500v2-fsl-linux-gnuspe"
Thanks,
Yiping