how can i build a integrated nor flash image like QorIQ_SDK_V2.0_P4080DS_20160527_NOR_Flash.bin

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how can i build a integrated nor flash image like QorIQ_SDK_V2.0_P4080DS_20160527_NOR_Flash.bin

891 Views
gaolixing
Contributor I

I program my p4080ds use the QorIQ_SDK_V2.0_P4080DS_20160527_NOR_Flash.bin,it is very convenient for me to program my board,i buile p4080 linux image by qoriq-components/yocto-sdk - Repo manifest for QorIQ Yocto SDK  project,i can build the linux image successfully,but i don't find one 128MB image like  QorIQ_SDK_V2.0_P4080DS_20160527_NOR_Flash.bin,how can i make it?

Labels (1)
0 Kudos
5 Replies

828 Views
gaolixing
Contributor I

thank you, i will try

0 Kudos

828 Views
Pavel
NXP Employee
NXP Employee
0 Kudos

827 Views
Pavel
NXP Employee
NXP Employee

It looks like a hex editor can be used for creation a binary file.

This binary file should include binary images of RCW, u-boot, FMAN microcode, uImage, .dtb and rootfile system.

See the Table 72 (NOR Flash Memory Map) in SDK 2.0-1703 documentation for the P4080ds board:

https://www.nxp.com/docs/en/supporting-information/QORIQ-SDK-2.0-IC-REV0.pdf

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

827 Views
gaolixing
Contributor I

thank you for reply,nor flash memory is clear from table 72,but which hex editor should be used,do you have a good recommendation? are there any documentation on how to do this

0 Kudos

827 Views
gaolixing
Contributor I

Why no one replied to me

0 Kudos