Unable to locate P1020RDB I2C pins

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unable to locate P1020RDB I2C pins

1,081件の閲覧回数
bilalwasim
Contributor II

I want to use the functionality of I2C (as well as SPI) on the P1020RDB board. However, seeing the schematics, I'm unable to locate the exact pins I should be using for I2C. In the schematics, it says that the U41D IC is responsible for dealing with I2C and SPI. However, on my board there is only U41, and not U41A, U41B etc. Seems to me that I have the wrong assembly diagrams. However, I'm unable to find any other reference manuals as well.

I'm using the P1020RDB with the Red casing, and not this one https://encrypted-tbn0.gstatic.com/images?q=tbn:ANd9GcRZqqsb1I5dUkv3cWx462t2nSWpXLuL-JBVwmpDfW4CtpoQ...

Any help would be appreciated.

ラベル(1)
タグ(1)
0 件の賞賛
返信
3 返答(返信)

874件の閲覧回数
ufedor
NXP Employee
NXP Employee

Please provide information printed on the case sticker and on-board sticker(s) and markings.

0 件の賞賛
返信

874件の閲覧回数
bilalwasim
Contributor II

Its P1020RDB RevD. There's a sticker on the back "SCH-26158 REV-D". I've got nothing else :smileysad:

0 件の賞賛
返信

874件の閲覧回数
ufedor
NXP Employee
NXP Employee

Please open a technical case to obtain the RDB schematics:

https://community.freescale.com/thread/381898

0 件の賞賛
返信