Question regarding initiate burst PCI Express transaction from Host CPU .(Using p1022).
As far as I understand CPU access to PCI memory will end-up in a 32bit or 64bit PCIE transfer requests.
Is it possible to create a read transaction of more then 64 bit (that will be implemented in one burst on the PCI Express)?
Is it possible to accomplish that with the DMA Controller where source address will point to a PCIE memory space?
Micha
已解决! 转到解答。
@ufedor @Micha_Yardeny
I'm using an LS1012A as an Endpoint and need to read large amounts of data from an RC. Performing memory-mapped reads using the core is working but extremely slow. I assume this is because the MRd TLPs are very small. Can you point me to any code examples showing the use of eDMA with PCIe, or even just a basic overview of how to achieve burst transactions?
Thanks,
Brett S.
Basically We have now that DMA working fine with 128 bytes payloads above PCI-E .
Can we theoretically increase DMA transfer size beyond the MPS (Maximum Payload Size)
Or in other works my question is can the host splits DMA transection to smaller TLP packets ?
If the answer is negative is that possible to go around it with limiting DMA band width BWC.?