Hardware Simulator

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Hardware Simulator

1,353 次查看
jm1015
Contributor II

Is it possible to simulate and test the code for testing peripherals without hardware? My intended processor is P1015/1024 QorIQ processor. I am using GHS multi V7 . Is there any software plug in which help users in develop application before they get actual hardware?

标签 (1)
3 回复数

1,059 次查看
alexander_yakov
NXP Employee
NXP Employee

Unfortunately, we do not offer software emulators to emulate P1015/1024 peripherals without hardware.


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,059 次查看
jm1015
Contributor II

Thank you, Alexander.

Is it also not possible to simulate and verify eTSEC module also?

* via loop back

Regards,

J Mathew

0 项奖励
回复

1,059 次查看
alexander_yakov
NXP Employee
NXP Employee

Unfortunately, we do not offer software emulator to emulate P1015/1024 eTSEC without hardware.