Hello community,
I am dealing with a problem with generating boot-image for following PowerPC/QorIQ Platforms:
- P2020
- T1042
My question is, can anybody give me some helpful info or links to information, how to generate an image for booting from SD card?
Especially, how to format sd card, where should be RCW placed, where PBL, U-Boot, DTB, and Linux ...?
Are there any tools or scripts under Linux/Yocto ..?
Thanks for the help!
Regards
Radek
已解决! 转到解答。
For the P2020 please refer to the NXP Linux SDK v1.9 Knowledge Center, 10.1 eSPI/SD/NAND Boot and 4.4.8.6.4 SD Deployment available at:
https://nxp.flexnetoperations.com/control/frse/download?agree=Accept&element=7126427
For the T1042 the NXP Linux SDK v2.0 is capable to generate complete SD card image (u-boot-sdcard) which has to be written to the SD card from offset block 8. For the deployment refer to the NXP Linux SDK v2.0 Documentation:
For the P2020 please refer to the NXP Linux SDK v1.9 Knowledge Center, 10.1 eSPI/SD/NAND Boot and 4.4.8.6.4 SD Deployment available at:
https://nxp.flexnetoperations.com/control/frse/download?agree=Accept&element=7126427
For the T1042 the NXP Linux SDK v2.0 is capable to generate complete SD card image (u-boot-sdcard) which has to be written to the SD card from offset block 8. For the deployment refer to the NXP Linux SDK v2.0 Documentation: