Don't work ethernet on P3041DS board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Don't work ethernet on P3041DS board

1,335 Views
alexanderkuznet
Contributor I

Hi all,

I have problem with P3041DS board. After reset I see next messages (from u-boot):

Fman1: Uploading microcode version 106.1.0

PHY reset timed out

PHY reset timed out

PHY reset timed out

PHY reset timed out

FM1@DTSEC1, FM1@DTSEC2, FM1@DTSEC3, FM1@DTSEC4, FM1@DTSEC5, FM1@TGEC1

And ethernet can't work.

What I can resolved this problem?

Labels (1)
0 Kudos
Reply
4 Replies

878 Views
oliver123
Contributor II

I have the exact same problem.  Did you solve your problem and how?

My P3041 is brand new, switches are set as in the documentation.

The Ethernet interfaces are not working on both U-boot and linux.

My u-boot version is 2011.12-00001

0 Kudos
Reply

878 Views
marius_grigoras
NXP Employee
NXP Employee

Do you use the RCW and fman-code binaries from SDK?

Marius

0 Kudos
Reply

878 Views
oliver123
Contributor II

Yes I use the the RCW and fman-code binaries from the SDK.

The problem was the ethact value in u-boot.

It was set to the wrong DTSEC interface. I used FM1@DTSEC5 instead of FM@DTSEC1.

0 Kudos
Reply

878 Views
hwrobel
NXP Employee
NXP Employee

Did it work before? If yes, what did you change? If not, does this mean the board's PHYs failed out of the box?

Triple check all your DIP switches on the board, go back to the default board configuration and use an unmodified default Freescale SDK image in the flash. That is known to work.

0 Kudos
Reply