Hi,
It's the first time I use a P2020 with a NAND Flash on the local bus, with the FCM.
NAND flash are new for me.
In the reference manual, the FCM use some RAM buffers.
I don't find where are located these buffers.. in DDR ? it's dedicated registers ? it's DMA ?
已解决! 转到解答。
Have a great day,
The FCM buffers SRAM is part of the P2020 local bus controller (eLBC). It is located on the P2020 chip. You can use this SRAM even in case when NAND chip (and/or any memory) is not connected to the P2020. In order to access this SRAM we should enable at least one eLBC bank assigned to the FCM (eLBC_BRn[MSEL] = 001 //FCM). Correspondingly eLBC_BRn[BA] defines base address of the SRAM.
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------