Are there any environments or OS'es that allow WIndows or .NET applications to run on Power cores?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Are there any environments or OS'es that allow WIndows or .NET applications to run on Power cores?

跳至解决方案
1,093 次查看
Larry5335
Contributor IV

Customer wants to run .NET applications on a e6500 core. It is preferred to run a form of Linux on the e6500 core.

Are there any forms of Linux or add-ons that run on Power that can support .NET based applications?

标签 (2)
标记 (3)
0 项奖励
回复
1 解答
894 次查看
Larry5335
Contributor IV

Looks like the open source world is working on a solution:

http://www.mono-project.com/docs/about-mono/

.NET Framework Class Library - The Mono platform provides a comprehensive set of classes that provide a solid foundation to build applications on. These classes are compatible with Microsoft’s .Net Framework classes.

在原帖中查看解决方案

0 项奖励
回复
3 回复数
895 次查看
Larry5335
Contributor IV

Looks like the open source world is working on a solution:

http://www.mono-project.com/docs/about-mono/

.NET Framework Class Library - The Mono platform provides a comprehensive set of classes that provide a solid foundation to build applications on. These classes are compatible with Microsoft’s .Net Framework classes.

0 项奖励
回复
894 次查看
ralftruebenbach
Contributor III

You could use a virtual i386 machine (e.g. qemu) and run wine or .NET for Linux in it. Don't know if this is really helpful but I think that's the closest you can get.

0 项奖励
回复
894 次查看
alexander_yakov
NXP Employee
NXP Employee

Sorry, we are unaware about any tools to run Windows or .NET applications to run on Power architecture.

I see .NET is available for several Linux distributions, still only x86/x64 architecture is supported.

.NET Downloads 


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复