Hi,
i couldn't find the operation amplifier on the NXP website.
the operation amplifier requirement as below:
->Channel: single channel
->VCC: 12V max
->output short current Isc : < 500 mA max, <=200mA is accept
->temperature: -40~125℃
->Slew rate: 50V/uS
->Package: SOT-23-5
-> Application: Automotive
only find some amplifier such as used in Audio-(Class D and Class AB ), Radio amplifier etc ,
they are not to meet the requirement, would you like kindly help to recommend some NXP amplifier or
share your comments, thanks.
Best regards.
Guofred
Solved! Go to Solution.
All of the Automotive PA focus on high power, you can get all of them below link:
All of the Automotive PA focus on high power, you can get all of them below link:
Hi @guoweisun ,
Thanks for your kindly help.
i would like to check it again, thanks.
Best regards.
Guofred