About the maximum input voltage of SA630D

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About the maximum input voltage of SA630D

403 Views
zjpp
Contributor I

I want to use SA630D as a switch for a square wave generator. Can the two input pins of this chip withstand a 7V, 1MHZ square wave?

0 Kudos
1 Reply

384 Views
diazmarin09
NXP TechSupport
NXP TechSupport

Hello,

I hope this response finds you well.

Do you mean INPUT and ENCH1 pins?

The primary function of the device is to switch signals in the frequency range DC to 1 GHz from one 50 Ω channel to another.

diazmarin09_0-1654808930354.png

 

Please note that this device is not recommended for new designs.

Regards,

David

0 Kudos