Hello.
I use MSC8156ADS board and Spartan 6 connected to it by SRIO. Data transfers go by Ocean DMA succesfully only if memory blocks on MSC8156 is non-cacheable. But if the source address of ocnDMA transfer configuration is set for cacheable memory ocnDMA transmith zeros(digital loopback shows same result). I try to sweep cache for this memory but it is all the same. I see cacheable memory filled with true data while debugging, but ocnDMA transmits zeros.
How can i transmit by ocnDMA from cacheable memory? Thank you.
#if (MSC815X_OCN_DMA0 == ON)
ocn_dma_init_params_t ocn_dma_init_params0 =
{
OCN_DMA_ID0,
OS_HWI_PRIORITY0,
{
/* On which core to enable the channel. */
ANY_CORE_ID, ANY_CORE_ID, ANY_CORE_ID, ANY_CORE_ID,
},
{
{
RIO0_ATMU_BASE,
DMA_ATMU_WIN_SIZE,
OCN_DMA_INTERFACE_RIO0
},
{
RIO1_ATMU_BASE,
DMA_ATMU_WIN_SIZE,
OCN_DMA_INTERFACE_RIO1
},
{
M3_BASE_ADDR,
DMA_ATMU_WIN_SIZE,
OCN_DMA_INTERFACE_LOCAL1
}
}
};
the OCN-DMA channel depend on core.and cachable data is private for core.you can think about it.