similar chip to HTSICH48 or HTSICH56 (ISO 14223 compatible)with a direct access to the user memory? (i.e- using SPI/CAN or other type of serial communication method)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

similar chip to HTSICH48 or HTSICH56 (ISO 14223 compatible)with a direct access to the user memory? (i.e- using SPI/CAN or other type of serial communication method)

384 Views
yigaledrey
Contributor I

Is there a chip similar to  HTSICH48 or  HTSICH56 (ISO 14223 compatible) but with a direct access to the user memory? (i.e- using SPI/CAN or other type of serial communication method) and on the other hand- have the RFID function?

Tags (2)
0 Kudos
Reply
0 Replies