similar chip to HTSICH48 or HTSICH56 (ISO 14223 compatible)with a direct access to the user memory? (i.e- using SPI/CAN or other type of serial communication method)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

similar chip to HTSICH48 or HTSICH56 (ISO 14223 compatible)with a direct access to the user memory? (i.e- using SPI/CAN or other type of serial communication method)

305 次查看
yigaledrey
Contributor I

Is there a chip similar to  HTSICH48 or  HTSICH56 (ISO 14223 compatible) but with a direct access to the user memory? (i.e- using SPI/CAN or other type of serial communication method) and on the other hand- have the RFID function?

标记 (2)
0 项奖励
0 回复数