pn5180, AN11802(rev 1.8) respberry pi 5, NfcrdlibEx1_DiscoveryLoop ... doesn's work

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

pn5180, AN11802(rev 1.8) respberry pi 5, NfcrdlibEx1_DiscoveryLoop ... doesn's work

跳至解决方案
438 次查看
jekim0109
Contributor II

As per AN11802 rev1.8 instructions, sw369328.zip was applied to raspberry pi 5, but the following error occurs.

 DiscoveryLoop Example:

Line: 133    Error - (0xF181) has occurred : 0xCCEE CC-Component ID, EE-Error code. Refer-ph_Status.h

Line: 142   Error - (0xF181) has occurred in NFCLIB

By any chance, isn't it a KERNEL SPI CFG DIR problem? Or is there a problem with SPI setting?

0 项奖励
回复
1 解答
427 次查看
jekim0109
Contributor II

I solved it.

Board_PiPn5180.h

 #define PHDRIVER_LINUX_USER_SPI

/*#define PHDRIVER_LINUX_KERNEL_SPI*/

在原帖中查看解决方案

2 回复数
428 次查看
jekim0109
Contributor II

I solved it.

Board_PiPn5180.h

 #define PHDRIVER_LINUX_USER_SPI

/*#define PHDRIVER_LINUX_KERNEL_SPI*/

416 次查看
danielchen
NXP TechSupport
NXP TechSupport

Thanks for your sharing.

0 项奖励
回复