Hello,
I'm using the NFC reader PN7642 to read and write data to the NHS3152 NFC Tag, and it works perfectly.
Additionally, I can utilize the NFC COCKPIT to configure the NFC field.
Specifically, I can access the VDDPA Setting from the DPC Calibration Onglet.
Now, I want to set the value of this VDDPA Setting from my source code,
but I haven't found a way to do it yet.
To address this issue, I attempted to locate all occurrences of the VDDPA setting within a project using the `grep` command.
Unfortunately, I couldn't find a way to set it.
Is it possible to set the VDDA value from the source code?
Thank you for your assistance.
Best regards,
Nobby
Hi
I can see the VDDPA in several files. For example, in file nfc_low_power_mode\ lpm.c
Regards
Daniel